Sharp Microelectronics - Sharp Microelectronics of the Americas (SMA) drives innovative LCD, optoelectronics, memory, imager, and RF components to market. The world's leading manufacturers of consumer and business technologies look to SMA for the products, expertise, and worldwide support they need to make their visions a reality. SMA, in Camas, Washington, is the microelectronics sales and marketing division of Sharp Electronics Corporation, a wholly owned subsidiary of Sharp Corporation.
- Product
Listing
- Featured
Products
- Tools
& Support
 | | GH04P21A2GE - Blue-Violet Laser Diode The GH04P21A2G makes full use of crystal growth technology developed for infrared, red, and blue-violet low-power laser diodes. In addition to a newly developed laser chip with a proprietary facet structure and a high power output of 210 mW that will contribute to high-speed recording for the next generation of DVDs, this current device also features a long service life of 10,000 hours, a level that leads the industry.
More... |
 | | GM5BW96320A and GM5BW96380A GM5BW96320A and GM5BW96380A offer high brightness with low power consumption. Sharp has announced the expansion of its family of white Light Emitting Diodes (LED) with two new devices (GM5BW96320A and GM5BW96380A) that can provide high brightness levels of 1400 and 2000 mcd at IF = 20 mA.
These new devices are ideally suited for many consumer and commercial lighting applications that up to now have used conventional incandescent bulbs or other technologies.
More... |
Brochures
Product Information
|
|