Power Relay FeatherWing Guide Datasheet by Adafruit Industries LLC

View All Related Products | Download PDF Datasheet
m e t S V. S Q m n r a m .0“ u r f a d a
Adafruit Power Relay FeatherWing
Created by lady ada
Last updated on 2018-08-22 03:55:34 PM UTC
2
3
6
6
7
8
9
9
9
9
Guide Contents
Guide Contents
Overview
Pinouts
Relay Control
Relay Output
Reset Button
Downloads
Datasheets & Files
Schematic
Fabrication Print
© Adafruit Industries https://learn.adafruit.com/adafruit-power-relay-featherwing Page 2 of 9
Overview
A Feather board without ambition is a Feather board without FeatherWings! This is the Power Relay FeatherWing. It
gives you power to control, and control over power. Put simply, you can now turn on and off lamps, fans, solenoids,
and other small appliances that run on up to 250VAC or DC power using any Feather board. Compared to our smaller
mini Relay FeatherWings (https://adafru.it/xDL), this one can handle a beefy 1200 Watts!
Using our Feather Stacking Headers (http://adafru.it/2830) or Feather Female Headers (http://adafru.it/2886) you can
connect a FeatherWing on top of your Feather board and let the board take flight. Check out our range of Feather
boards here. (https://adafru.it/mf2)
This Wing has a non-latching type relay. You can switch up to 10A of resistive-load current at 120VAC, 5A at 240VAC.
© Adafruit Industries https://learn.adafruit.com/adafruit-power-relay-featherwing Page 3 of 9
With Inductive Ioads, about halfmat. Check the datasheet forthe relay for the exact switching capacity, as It depends IIIIII IIII ilMIllIIIIIIIIIIIIHHHHHHIHHIIII O 000000000000 Fouer Delag It“: Featherluinq omrzon GSLE-14 3V DC: QNC ' W 5 A 150 V AC 1254W9 A H H HHHH H HHHH III'I"II‘HI|‘I|
With inductive loads, about half that. Check the datasheet for the relay for the exact switching capacity, as it depends
on type of load and voltage type and magnitude. This relay is good for handling fairly large devices, computers, TVs,
small appliances and more.
However, note that when closing the relay, it will draw 100mA continuously from the 3.3V power rail
Each FeatherWing comes with a fully assembled and tested PCB, header you can use to attach to your Feather. By
soldering closed the jumper on the underside of the Wing you can select which pin you want to use for the relay
control. Some light soldering is required.
© Adafruit Industries https://learn.adafruit.com/adafruit-power-relay-featherwing Page 4 of 9
O O Pouer Relaq # V Fenheruiy .1 01'." Eggntzmza“ feat' Ier Shun . ,u n: O Conn-cl pm nun-l 9 ,, Jooofifiégfiofmo o r- -« 3 a: m
Please note: If using with high voltages (> 24V) use care and common sense! High voltages require experience, and
are only for use by engineers who are comfortable with guidelines and know how to use them safely!
© Adafruit Industries https://learn.adafruit.com/adafruit-power-relay-featherwing Page 5 of 9
oooooooooooo Power Relau . Featheruinq QmROn [m ® GSLE-14 ‘ m z-zx E i 'l l i 1.4 l1“ m I ‘ *smg: ‘1254W9 é; ‘(D56065Ouv‘ r 000000000000 Pouor Relag Featheruing/ “.munnmwuu‘
Pinouts
Relay Control
Controlling the relay is really simple. The relay uses a single pin for control. When floating or pulled low, the relay is
'open' or unset. When the pin is pulled high, the relay switches closed/set. A red LED next to the pin will let you know
that the signal is high. You will need to solder closed a jumper on the bottom to match the pin you want to use for
control.
When the relay is closed it will draw approximately 100 milliamps (yep! its a big relay and the voltage is only 3.3V) so
keep that in mind when using a lot of accessories, sensors and devices on the 3.3V power line.
© Adafruit Industries https://learn.adafruit.com/adafruit-power-relay-featherwing Page 6 of 9
OOOOOOBDOOOOOO . Relago 8"\ $9.. ngtegeruinqer U Z E SE- ég: o-muv f 8 3 Ag somrstzstza“ ea [(5)1 Shun a jump-er lo f’ 0 connect pin I. signal 9:-” QIE] 0 \‘0000000000000000 Q 000000000000 Pouer Relag ‘,.__,_ ,flflwm _ n— Featheruing 1 omnon ‘ l ‘ GSLE-14 3VDC= &%@ 10A250VA( 5A250VA( 1’ I254W9 A; O 66o58ooouw n “77;,
Relay Output
The Wing has the power control output on the end, a 3-pin 5.08 mm terminal block. The COM pin is what you should
connect the signal you're planning to switch.
If the relay is unset, the NC pin (Normally Connected) is mechanically connected to COM. NO (Normally Open) is
mechanically disconnected.
When the relay is set, NC becomes disconnected from COM and NO is connected to COM
© Adafruit Industries https://learn.adafruit.com/adafruit-power-relay-featherwing Page 7 of 9
(d 000000000000 I ‘ , . , , Pouer Relag ‘ ”Featheruinqer \ ‘ '- PE. 5; I maeazrzgrgu fea Short a jump-er la ['19 connect pin I. signal , i'O 'oooooggloogggoooéo 000000000000 Pouer Relag _7 _.~ Featheruing EM omnofl l-® 1 GSLE-14 - ' svoc= mass HAZEL/AC suzsoVAc o: *1254W9 E05‘: 606” 000
Reset Button
There is a Reset button on both Wings, this is connected to the RST pin and will short it to ground. It is not connected
to the relay at all, its handy for restarting your Feather
© Adafruit Industries https://learn.adafruit.com/adafruit-power-relay-featherwing Page 8 of 9
o o a” a
Downloads
Datasheets & Files
EagleCAD PCB files on GitHub (https://adafru.it/pXB)
Fritzing object in Adafruit Fritzing library (https://adafru.it/c7M)
Datasheet for the Relay (https://adafru.it/pXC)
Schematic
Fabrication Print
Dims in inches
© Adafruit Industries Last Updated: 2018-08-22 03:55:28 PM UTC Page 9 of 9

Products related to this Datasheet

POWER RELAY FEATHERWING