Designing Thermocouple Applications with a sensor AFE

作者:Jason Seitz

資料提供者:Convergence Promotions LLC


A simple thermocouple, combined with an analog front end, can provide a more robust, lower cost, wider-range alternative to other temperature sensors.

In 1821, Thomas Seebeck discovered the physical phenomenon that when two dissimilar metals are joined on both ends and one end is heated, a continuous current is created in the thermoelectric circuit.¹ If the other end is broken, a voltage can be measured that is proportional to the temperature difference between the heated junction (measuring or "hot" junction) and the open end (reference or "cold" junction) at which the measurement is taken. This physical property, called the Seebeck effect, is the basis of the thermocouple sensor.

Thermocouple sensors have several advantages that make them popular in many applications such as industrial, medical, and home appliances. Compared to other popular temperature sensors, such as Remote Temperature Diodes (RTDs), thermistors, and IC sensors, thermocouples are more rugged, less expensive, and can operate over the largest temperature range. Furthermore, thermocouples are passive sensors and thus don't require an electrical stimulus to operate, which minimizes system complexity. Along with their many benefits, it's important to fully understand thermocouples' electrical characteristics when designing with them.

Thermocouple sensors are categorized by different calibration types (e.g., type K and type J) based on types of dissimilar metals which are used to form the thermocouple junction. Based on its calibration type, each thermocouple sensor has a sensitivity (µV/C°), a temperature range, and a non-linear voltage curve over that temperature range. For example, a type K thermocouple has an average sensitivity of approximately 41 µV/°C and an operating range of -200 to 1,250 °C. Thermocouple voltage curves are non-linear over their operating temperature ranges, as can be seen in Figure 1.

Figure 1: Thermocouple output voltage versus temperature.

Figure 1: Thermocouple output voltage versus temperature.

When designing with thermocouples, it's important to understand that they are bipolar, which means they can produce a positive or a negative voltage depending on whether or not the measured temperature is higher or lower, respectively, than the system temperature.

As mentioned earlier, the voltage created by a thermocouple is relative to the temperature difference between the measuring junction, which is placed in the measured environment, and the reference junction, which is typically in the measuring system environment. This means that the thermocouple is only capable of recognizing a temperature difference between two points and does not have the ability to measure absolute temperature. To determine the absolute temperature of the measured environment, it's necessary to determine the temperature of the reference junction and factor it in to the absolute temperature calculation. This technique is called "cold junction compensation," and can be handled by placing a temperature sensor, such as National Semiconductor's LM94022, in the measurement system close to the reference junction. This temperature sensor should have an isothermal connection to the board to minimize any potential temperature gradients.

Depending on the temperature range and the accuracy requirements of the application, it's often necessary to amplify the thermocouple signal before system processing by an Analog-to-Digital Converter (ADC) or a Microcontroller (MCU). A popular thermocouple amplifier configuration is a differential amplifier. One benefit of a differential amplifier is minimizing the effects of common-mode pickup, which can be quite significant across a long thermocouple wire in a noisy environment. Another benefit of a differential amplifier is the ability to level-shift a signal in order to avoid input saturation by staying within the input common-mode range of the amplifiers. This is beneficial in thermocouple applications where it is necessary to measure temperatures close to or below the system temperature.

Figure 2: Thermocouple sensor AFE.

Figure 2: Thermocouple sensor AFE.

Traditionally, system designers have designed thermocouple measurement systems using discrete amplifiers, ADCs, and passive components. An attractive alternative to discrete custom designs is National Semiconductor's LMP90100. The LMP90100 is a highly integrated, multichannel, low-power 24-bit sensor Analog Front End (AFE). The device features a precision, 24-bit Sigma Delta ADC with a low-noise programmable gain amplifier and a fully differential high impedance analog input multiplexer. Higher integration coupled with precision performance make the LMP90100 a natural fit for thermocouple applications (see Figure 2).

Amplifier specifications that are critical for thermocouple applications include low-offset error, low-RMS noise, and high Common-mode Rejection Ratio (CMRR). Since the typical output voltage of a thermocouple is in the µV range, it is crucial that offset voltage remain small and insignificant relative to the measured signal. To satisfy this requirement, the LMP90100 features true continuous background calibration for offset and gain. The true continuous background calibration of the LMP90100 essentially eliminates offset and gain errors across temperature and time for all gains and sample rates, providing measurement accuracy without sacrificing speed and power consumption. The net result is a precision solution with a typical offset voltage of 8.4 nV and a temperature drift of 0.125 nV/°C. Similarly, having an amplifier with low noise and a high CMRR will improve accuracy and reduce the potential effects of common-mode pickup. The LMP90100 offers noise less than 10 µV RMS and has a high 117 dB CMRR.

In addition to the LMP90100's precision performance, the sensor AFE offers rail-to-rail input and integrates sensor diagnostics. Rail-to-rail input capability allows designers to capture near ground signals, providing the best opportunity to measure temperatures that are at, or very near, the system ambient temperature. Sensor diagnostics allow the detection of open and short circuit conditions and out-of-range signals, without requiring user intervention, resulting in enhanced system reliability.

Thermocouples are popular because they are inexpensive, rugged, and operate over an extended temperature range. When designing with thermocouples, keep in mind the specific type, associated sensitivity, and the fact that they are bipolar devices. A differential amplifier configuration is a popular circuit that allows good CMRR performance. Depending on specific measurement requirements, developers may need to add level shifting to the circuit. Due to its low-noise, low-offset voltage, high CMRR, and rail-to-rail input capability, National's LMP90100 sensor AFE makes for a good fit in a thermocouple application.

References
  1. OMEGA Temperature Measurement Handbook (2007): Z-21.
Convergence Logo

聲明:各作者及/或論壇參與者於本網站所發表之意見、理念和觀點,概不反映 DigiKey 的意見、理念和觀點,亦非 DigiKey 的正式原則。

關於作者

Jason Seitz

Article authored by Jason Seitz of National Semiconductor.

關於出版者

Convergence Promotions LLC