Peripheral Reflex System Avoids MCU Overload
資料提供者:Convergence Promotions LLC
2011-04-06
Normally, MCUs spend much of their time passing information between peripherals. That doesn’t have to be the case.
The Peripheral Reflex System (PRS) is a network which lets the different peripheral modules communicate directly with each other without involving the CPU. Peripheral modules which send out Reflex signals are called producers. The PRS routes these reflex signals to consumer peripherals which apply actions depending on the Reflex signals received. The format for the Reflex signals is not given, but edge triggers and other functionality can be applied by the PRS.
Overview
An overview of one channel and how four different peripherals can be connected using PRS is given in Figure 1. The PRS contains eight interconnect channels, and each of these can select between all of the output Reflex signals offered by the producers. The consumers can then choose which PRS channel to listen to and perform actions based on the Reflex signals routed through that channel. The Reflex signals can be both pulse signals and level signals. Synchronous PRS pulses are one HFPERCLK cycle long, and can either be sent out by a producer (e.g. ADC conversion complete) or be generated from the edge detector in the PRS channel. Level signals can have an arbitrary waveform, but will be synchronized with the HFPERCLK.
Figure 1 shows four peripherals connected to two PRS channels. On one channel is TIMER0 and ADC0 and the ACMP and TIMER1 are connected to a second channel. An overflow from TIMER0 can start an ADC single conversion and an ACMP output can be used as input for a Compare/Capture channel on TIMER1.
![]() |
| Figure 1: PRS overview. |
General operation
Channel functions
Different functions can be applied to a Reflex signal within the PRS. Each channel includes an edge detector to enable generation of pulse signals from level signals. It is also possible to generate output Reflex signals by software writing to PRS_SWPULSE and PRS_SWLEVEL registers. PRS_SWLEVEL is a programmable level for each channel and holds the value it is programmed to. The PRS_SWPULSE will give out a one-cycle high pulse if it is written to 1, otherwise a 0 is asserted. The SWLEVEL and SWPULSE signals are then XOR’ed with the selected input from the producers to form the output signal sent to the consumers listening to the channel. This is illustrated in Figure 1.
The efm32lib function void PRS_SourceSignalSet(unsigned int ch, uint32_t source, uint32_t signal, PRS_Edge_TypeDef edge) can be used to easily configure the PRS channels. By specifying the PRS channel producing peripheral signal from the peripheral and the edge for pulse generation, the function configures the PRS accordingly.
Producers
Each PRS channel can choose between signals from several producers, which is configured in SOURCESEL in PRS_CHx_CTRL. Each of these producers outputs one or more signals which can be selected by setting the SIGSEL field in PRS_CHx_CTRL. Setting the SOURCESEL bits to 0 (Off) leads to a constant 0 output from the input mux. An overview of the available producers is given in Table 1.
|
Module |
Reflex Output |
Output Format |
|
ACMP |
Comparator Output |
Level |
|
ADC |
Single Conversion Done |
Pulse |
|
Scan Conversion Done |
Pulse |
|
|
DAC |
Channel 0 Conversion Done |
Pulse |
|
Channel 0 Conversion Done |
Pulse |
|
|
GPIO |
Pin 0 Input |
Level |
|
Pin 1 Input |
Level |
|
|
Pin 2 Input |
Level |
|
|
Pin 3 Input |
Level |
|
|
Pin 4 Input |
Level |
|
|
Pin 5 Input |
Level |
|
|
Pin 6 Input |
Level |
|
|
Pin 7 Input |
Level |
|
|
Pin 8 Input |
Level |
|
|
Pin 9 Input |
Level |
|
|
Pin 10 Input |
Level |
|
|
Pin 11 Input |
Level |
|
|
Pin 12 Input |
Level |
|
|
Pin 13 Input |
Level |
|
|
Pin 14 Input |
Level |
|
|
Pin 15 Input |
Level |
|
|
RTC |
Overflow |
Pulse |
|
Compare Match 0 |
Pulse |
|
|
Compare Match 1 |
Pulse |
|
|
TIMER |
Underflow |
Pulse |
|
Overflow |
Pulse |
|
|
CCO Output |
Level |
|
|
CC1 Output |
Level |
|
|
CC2 Output |
Level |
|
|
UART |
TX Complete |
Pulse |
|
RX Data Received |
Pulse |
|
|
USART |
TX Complete |
Pulse |
|
RX Data Received |
Pulse |
|
|
IrDA Decoder Output |
Level |
|
|
VCMP |
Comparator Output |
Level |
Consumers
Consumer peripherals (Table 2) can be set to listen to a PRS channel and perform an action based on the signal received on that channel. Most consumers expect pulse input, while some can handle level inputs as well.
| Module | Reflex Input | Input Format |
| ADC | Single Mode Trigger | Pulse |
| Scan Mode Trigger | Pulse | |
| DAC | Channel 0 Trigger | Pulse |
| Channel 1 Trigger | Pulse | |
| TIMER | CCO Input | Pulse/Level |
| CC1 Input | Pulse/Level | |
| CC2 Input | Pulse/Level | |
| DTI Fault Source 0 (TIMER0 only) | Pulse | |
| DTI Fault Source 1 (TIMER0 only) | Pulse | |
| DTI Input (TIMER0 only) | Pulse/Level | |
| UART | TX/RX Enable | Pulse |
| USART | TX/RX Enable | Pulse |
| IrDA Encoder Input (USART0 only) | Level |
Software examples
This section describes four software examples that explore possible interactions between peripherals using the PRS:
- TIMER triggered ADC conversion
- Pulse Width Measurement with the ACMP and TIMER
- GPIO triggered UART transmission
- Software triggered DAC conversion
Figure 2 shows how to set up ADC0 to start a single conversion every time that TIMER0 overflows. TIMER0 sends a one HFPERCLK cycle high pulse sent from TIMER0 to the ADC0 through the PRS on each overflow, and the ADC does a single conversion which is displayed on the LCD of the STK/DK development boards. The ADC consumes pulse signals, which are the same signals produced by the TIMER. In this case there is no edge detection needed, so the PRS leaves the incoming signal unchanged.
![]() |
| Figure 2: TIMER0 overflow starting ADC0 single conversions using the PRS. |
The ADC is configured with 8-bit resolution and Vdd as both reference and input. When the ADC finishes the conversion it generates a single conversion complete interrupt. The CPU will then fetch the result and display it on the LCD. The displayed result is a direct reading from the ADC0_SINGLEDATA register which is always 255, given that the input is the same as the reference. The DMA can also be used to fetch the conversion result and that is covered by the AN0021 Analog to Digital Converter.
The software project
prs_timer_adc implements this example and can be used on both STK and DK development boards.Pulse width measurement with ACMP and TIMER
Figure 3 illustrates how to measure the pulse width or period of an arbitrary waveform. The ACMP is used to send a level signal through the PRS. TIMER0 consumes both pulse and level signals so the PRS leaves the incoming signal unchanged. On TIMER0 the PRS signal is used as input for CC0 channel. TIMER0 starts counting on a positive edge and captures the counter value on a negative edge.
Figure 3 also shows the level output from the ACMP sent through the PRS to the TIMER which measures the pulse width using the capture feature.
The software project
prs_pulse_width implements this example and can be used on both STK and DK. To trigger the pulse width measurement, pin PC4 (P4.7 on the DK protoboard) must be connected to VMCU to generate a high level that will trigger the ACMP and start the TIMER. When the connection is released, the output of the ACMP will be low again and the TIMER captures the counter value and displays it on the LCD.![]() |
| Figure 3: ACMP level output used as PRS signal for TIMER0 CC0 channel input. |
GPIO triggered USART transmission
Figure 4 illustrates how to use an external signal coming through the GPIO to enable the USART transmitter. It shows a positive edge from a GPIO pin sent on the producer side through the PRS edge detector to create a one HFPERCLK cycle pulse on the consumer side. The GPIO produces level signals which are not consumed by the UART so the edge detector must be used to generate a pulse signal on a GPIO positive edge transition. The clock pulse enables the USART TX and transmits the data that was placed in the TX buffer. For the GPIO to generate PRS signals, the PRS Sense must be enabled in the GPIO_INSENSE register.
The software project
prs_gpio_uart implements this example and is intended for the DK only. To enable the USART TX, pin PD0 must be connected to VMCU to generate a positive edge. The EFM32 will then send the character ‘X’ through SERIAL A with a 57600 baud rate, no parity and one stop bit.![]() |
| Figure 4: USART TX enabled by GPIO signal using the PRS. |
Software generated PRS pulse triggers DAC conversion
Figure 5 shows how to generate a PRS pulse by software. The PRS pulse will trigger a DAC conversion which outputs a 0.5 V signal on pin PB11. It is possible to generate both pulse and level signals by software. In this case a pulse signal is generated because it is the type of signal consumed by the DAC. DAC conversions can also be started by software in the DAC itself. This example only shows how this can be done through the PRS as well.
![]() |
| Figure 5: Software triggered PRS signal. |
Figure 5 shows a one HFPERCLK cycle pulse triggered from software. Pulse and level signals can be generated by software by writing directly to the PRS_SWPULSE and PRS_SWLEVEL registers respectively. They can also be generated using functions from the efm32lib:
void PRS_PulseTrigger(uint32_t channels)generates pulse signalsvoid PRS_LevelSet(uint32_t level, uint32_t mask)generates level signals
prs_soft_dac implements this example and can be used on both STK and DK.Monitoring of PRS signals
The PRS channels can be monitored using peripherals that consume PRS signals. One example is using a TIMER to make a capture when there is activity on the PRS channel it is connected to. The software project
main_prs_channel_scan exemplifies how this can be accomplished and can be used on both STK and DK.The
function PRS_ScanChannel(TIMER_TypeDef *timer, TIMER_PRSSEL_TypeDef prsCh, TIMER_Edge_TypeDef edgeType) in the main_prs_channel_scan project can be used to monitor activity on a specific PRS channel. It sets the CC0 channel on the chosen TIMER to capture a selected signal edge. The project can be used on both STK and DK and the parameters are as follows:timer:pointer to the TIMER peripheral register c\blockprsCh:PRS channel to be monitorededgeType:signal edge to be monitored/captured
Another option is to have a capture interrupt instead of polling. That way the program will not hang and the processor will be available to execute other tasks. When a capture is triggered, the user knows that there was activity on the selected PRS channel.
聲明:各作者及/或論壇參與者於本網站所發表之意見、理念和觀點,概不反映 DigiKey 的意見、理念和觀點,亦非 DigiKey 的正式原則。