Semtech Power Supplies 101

作者:DigiKey Technical Content

資料提供者:DigiKey

In the most basic terms, a step-down regulator takes an input voltage and converts it to a lower voltage required by the load. There are two major types of voltage regulators, linear and switching. A linear regulator works by absorbing the energy difference between the input and the output while a switching regulator chops the input voltage and then averages the chopped voltage to provide the proper output voltage.

A voltage regulator which is placed close to the device or devices for which it is powering is commonly referred to as a point of load regulator. This type of regulator often receives its input from a voltage bus contained on the PCB.

There are several parameters that should be considered when evaluating power supplies for particular applications.

  • Quiescent Current – The amount of current an IC consumes when it is not source current and its inputs are not cycling.
  • Efficiency – Defined as the ratio of power into a regulator circuit to the output power delivered by the regulator.  Power input includes quiescent currents, losses due to parasitic components and power delivered to the load.
  • Equivalent Series Resistance – The resistive component of the capacitors used in a regulator circuit. Attention needs to be paid to the ESR of the capacitors of the output.
  • The Loop – Defined as all the elements affecting the output and stability of a regulator. This includes such blocks as the power stage, error amplifier, modulator, and compensation circuits.

Additionally, as illustrated in Figure 1, several other specifications associated with power supplies affect their operation.

  • TJ-MAX - The highest allowable temperature the junction in the IC is allowed to achieve.
  • TA - Defined as the ambient temperature of the air in the vicinity of the regulator.
  • RTHETA-JA - The thermal resistance from the junction to ambient. This includes the thermal resistance from the junction-to-case, the case-to-PCB, and PCB-to-air.
  • VFB - The feedback voltage used to set the output voltage. R1 and R2 create a resistor divider to form VFB from VOUT. The error amp works to keep VFB equal to VREF.
Image of voltage regulator definitions

Figure 1: Voltage regulator definitions.

Linear regulators are often used because of their ease of use and typically have a very low component count requirement. This type of regulator is equivalent to an adjustable resistor which drops VIN to VOUT and tries to keep VOUT constant. The following is a list of key parameters to look for in a linear regulator:

  • Dropout Voltage – This is the minimum voltage needed above VOUT to maintain proper regulation.
  • Low Drop Out (LDO) – This is a type of regulator which functions when VDROPOUT is very small.
  • Stability Region – The area of a linear regulator where the output will remain stable. It is given for different output capacitances and depends on the ESR of the output capacitor.
  • PD-MAX - The maximum power a device can dissipate is given by. It is defined as the difference of TJ-MAX and TAMBIENT divided by RTHETA-JA. It is possible to figure out what the maximum allowable output current is by combining and rearranging the power dissipation equations.

Linear regulators can be classified as either integrated or discrete (as illustrated in Figure 2). An integrated linear regulator has the pass element integrated in the package. A discrete solution has an external pass element. Feedback components may or may not be integrated for either a discrete or integrated regulator. The SC339 is an example of a discrete linear regulator. The SC4215H is an example of an integrated linear regulator.

Image of integrated vs. discrete linear regulators

Figure 2: Integrated vs. discrete linear regulators.

In the example shown in Figure 3, the VIN has been defined to be 3.3 V and VOUT has been defined as 2.5 V. We begin by selecting R2 to be 10 kΩ. From the equation for calculating R1 and using the value of 0.5 V for VREF from the datasheet, we come up with a value of 40 kΩ needed for R1. We have defined the TAMBIENT to be 50°C. From the datasheet, we find the value for TJ-MAX defined as 125°C and RTHETA-JA defined as 36°C/Watt. With those values, we can calculate the maximum available output current, which is 2.6 A.

Image of linear regulator example – SC4216H

Figure 3: Linear regulator example – SC4216H.

The datasheet states 10 μF per Amp of output current is needed to prevent the input to the regulator from sagging. To support the full current calculated on the previous slide, a minimum of 26 μF is needed. Due to capacitor tolerances, a minimum of 33 μF capacitor should be chosen. In addition to the bulk cap, a 4.7 μF ceramic is recommended to be placed directly next to the VIN pin of the regulator. For the output, the same rule of 10 μF per amp of output current is recommended. This will lead to the same value of 33 μF being used for the output. It is important to watch the ESR of the output capacitor to ensure the regions of instability are not entered.  While a graph is not given for a 33 μF capacitor, we can interpolate between the two graphs given and use a 5 mΩ ESR to maintain stability. It is also recommended to use a 0.1 μF capacitor next to the VOUT pin.

A buck regulator converts a higher VIN to a lower VOUT as shown in Figure 4. The controller opens and closes switch S periodically to connect the phase node between VIN and ground. The waveform seen at the phase node is then filtered through the inductor and capacitor to provide a smooth voltage to the load.

Image of buck regulator

Figure 4: Buck regulator.

The buck regulator has two different states (as shown in Figure 5), when switch S is closed and when switch S is open. When the switch is closed, VIN charges the inductor and capacitor and supplies the output current. When the switch is open, the magnetic field in the inductor collapses and causes the voltage across the inductor to change polarity. This change in polarity pulls the phase node below ground, forward biasing the diode. This allows current to continue to flow as the inductor sources the current needed by the load.

Image of basic buck regulator states

Figure 5: Basic buck regulator states.

As mentioned previously, the diode becomes forward biased with the collapsing of the magnetic field of the inductor. This occurs without any reference to a clock and is known as an asynchronous regulator. The VF of the diode used represents a significant portion of losses within an asynchronous regulator, especially as the value of VF approaches the value of VOUT. By replacing the diode with another MOSFET, the losses in the system can be reduced. This requires a more complex controller to ensure the MOSFETs are not both turned on at the same time. Since the bottom MOSFET is now controlled, the topology is referred to as a synchronous regulator. S1 is also known as the top FET or the high-side FET. S2 is also known as the bottom FET or the low-side FET. The comparison between the Asynchronous and Synchronous Buck Regulators is shown in Figure 6.

Image of asynchronous vs. synchronous buck regulators

Figure 6: Asynchronous vs. synchronous buck regulators.

The waveforms on Figure 7 are associated with a buck regulator. DH is the control signal to the high-side FET. As the controller turns on the high-side FET, current ramps up in the switch. At the same time, current also ramps up in the inductor and the voltage of the phase node hits VIN. When the high-side switch is turned off, current ramps down in both the inductor and the low-side FET and the voltage at the phase node is pulled to ground.

The signal at VPHASE is then filtered to form VOUT.

The amount of time the high-side FET is on is defined as tON. The amount of time the high-side FET is off is defined as tOFF. The time of tON plus tOFF is defined as T or total cycle time.

Image of basic buck regulator waveforms

Figure 7: Basic buck regulator waveforms.

Buck regulators can be further divided into two classes (as depicted in Figure 8), integrated regulators and switching controllers. The integrated switching regulator builds the FETs into the package or in the silicon. The switching controller requires switches to be placed external to the IC.

Image of integrated switching regulator vs. switching controller

Figure 8: Integrated switching regulator vs. switching controller.

Voltages other than the fixed options provided can be used so long as a feedback network is added to design. It is recommended to use the 1 V SC189 when requiring voltages other than the standard fixed voltages. Due to the internal compensation, the use of a capacitor across the top side of the feedback network is necessary to maintain stability.  The equation for calculating the capacitor was already discussed. VOUT is the desired output voltage and VOSTD is the voltage of SC189 with no feedback network. The feedback resistors are calculated via the formula found on Figure 9. The VREF to be used in the equation is the VOSTD of the part or 1 V when the recommended SC189A is used.

Image of feedback resistors calculation formula

Figure 9: Feedback resistors calculation formula.

In summary, the best time to use a linear regulator is when noise in the system cannot be tolerated or when the VIN and VOUT difference is small. The best time to use a switching regulator is when the difference between VIN and VOUT is large. Also, it is best to use a switching regulator when efficiency is important and large currents are involved. Semtech has many options for both linear regulators and switching regulators.

References

  1. For a full audio version of this training please visit: Power Supplies 101
 
DigiKey logo

聲明:各作者及/或論壇參與者於本網站所發表之意見、理念和觀點,概不反映 DigiKey 的意見、理念和觀點,亦非 DigiKey 的正式原則。

關於作者

DigiKey Technical Content

關於出版者

DigiKey

DigiKey 總部位於美國明尼蘇達州錫夫里弗福爾斯市,是全球化的全方位服務供應商,能夠滿足電子元件的原型開發/設計以及量產需求,並透過 DigiKey 網站提供超過 750 家優質知名品牌製造商的 650 多萬款產品。