Tips on Developing an Energy-Harvesting Power Budget

作者:Bill Schweber

資料提供者:Electronic Products

Data-acquisition systems that use energy harvesting (EH) for all of their operating power are increasingly popular, made possible by a combination of extremely low-power components for power management, energy storage, data processing, sensor interfacing, and the wireless radio link.

However, designing a viable energy-harvesting system is difficult and takes more than just extensive use of energy-efficient components. It needs careful planning, analysis of operating sequences and timing and understanding of trade-offs, as there are two different, asynchronous, uncorrelated processes occurring. First, collecting and storing random clumps of energy (joules or Whr), which is primarily a random process; then, spending energy via a set schedule, mostly in short bursts of power (W), the rate at which the energy is used. Of course, the total energy used must be less than the amount of energy you have accumulated, and the peak power needs must be within the capacity of the system to deliver it.

How much energy, anyway?

It is simplistic but misleading to think that using harvested power as a source is obtaining "something for almost nothing." First, both the amount of energy impinging on the transducer, and the amount it can actually produce is low, even if 100% efficient.

Second, the reality is that not only are most such sources sporadic, but also the transducers are very inefficient at converting the impinging energy into electrical energy, and this does not take into account losses within the electronics themselves. Generally, less than 10% of the energy reaching the transducer actually ends up in an energy-harvesting battery or supercapacitor for later use, whether the energy is from wind, solar, vibration, sound, RF, or thermal transducers. Table 1 shows some sample numbers. (Note: These are just order-of-magnitude approximations.)

Source Source Power Harvested Power

Light - Indoor

0.1 mW/cm²

10 μW/cm²

Light - Outdoor

100 mW/cm²

10 mW/cm²

Vibration/Motion - Human

0.5 m at 1 Hz
1 mW at 50 Hz

4 μW/cm²

Vibration/Motion - Machine

1 mW at 5 Hz
10 mW at 1 kHz

100 μW/cm²

Thermal - Human

20 mW/cm²

30 μW/cm²

Thermal - Machine

100 mW/cm²

1 to 10 mW/cm²

Table 1: The amount of available power from various harvesting sources is very low, and the net power harvested is far lower.

A major up-front part of the design is working through the power and energy budget. While this seems to be an obvious statement, it is both more complicated and more important in energy-harvesting design than for many other types of design. There are several reasons for this:

  • EH-based designs operate intermittently, at very low duty cycles. It is critical to budget and balance energy and power used between the amount of time a function is active and thus using the maximum, versus the power it uses. Is it better to use shorter bursts which consume more power, or longer, lower-power bursts of activity?
  • It is not just a matter of quiescent versus active energy/power. You have to look at use during sleep mode, wakeup time (and clock cycles), and other transitional events (Figure 1).

Microchip Calculating average system power consumption

Figure 1: Calculating average system power consumption. (Courtesy of Microchip.)

  • It is challenging to measure used energy/power. Since the system is operating in the nanoampere and microampere range most of the time, only occasionally reaching milliamperes and higher, conventional current-measurement instrumentation will not work (more on this shortly in the section "What about testing?").
  • The wireless transmission phase is usually the most energy-intensive period. It requires analysis of the trade-offs among the factors of power used, transmission frequency, data packing, link errors, format, protocol, possible retransmission, and amount of data to be sent. In almost all cases, this function is purchased "as is" from an external vendor due to regulatory, spectrum, protocol, packaging, and other complex wireless issues rather than being designed by the team doing the harvesting/data part of the design.
Be tough, but also open-minded when looking at the budget. Ask yourself what is available and what is needed. Certainly go with the lowest power affordable components that will meet your needs, but also balance this factor against the time period of use. If the active/sleep mode power-use ratio is 100:1, for example, and the duty cycle is 1%, that is the same power usage as 200:1 ratio and a 0.5% duty cycle (there actually is a small difference between the two if you do the math carefully and take into account the round-off approximation, but our example is deliberately a simplification). Transitions between operating phases then become critical parts of the analysis.

When doing the budget, do not ignore the obvious: many ICs characterize their cycles by current needed, but designers must look at both energy and power used, since the energy-harvesting supply must have the capacity to provide the overall energy and at the burst-power levels needed.

Doing the budget

A typical EH-based wireless application will need a few hundred milliseconds or less to complete the sensor data collection and transmission phase. For most applications that monitor real-world processes, it is more likely that readings are actually needed every few minutes or hours, rather than every few seconds. Consequently, wireless sensors exhibit an activity profile characterized by prolonged quiescent/deep-sleep states interrupted periodically by bursts of activity.

A budget and energy/power analysis can start with a basic spreadsheet containing two sections. The simpler side shows the energy-collection budget, including losses in accumulation, storage, and management. The more complex side defines minimum/maximum values for power consumption in various operational stages, and evaluates what-if analysis versus time in each mode. Use this activity profile to assess the trade-offs of using lower-power parts and modes versus time in each mode, for both performance responsiveness and energy use.

In general, lower-clock-speed operation also implies lower energy/power consumption, and so may seem attractive. But go through the numbers carefully: with a higher clock speed, the system may be able to wake up, complete the data analysis and transmission, and go into its extreme low-power sleep mode more quickly and with less overall energy use.

A look at a representative microcontroller shows some of the numbers involved. The EFM32 Tiny Gecko family from Energy Micro AS (Figure 2) is based on the 32-bit ARM® Cortex™ architecture and includes various combinations of Flash and RAM memory.

The EFM32 Tiny Gecko family from Energy Micro

Figure 2: The EFM32 Tiny Gecko family from Energy Micro (shown here as part of a starter kit) demonstrates the extreme low-power operation of EH-compatible microcontrollers, with various operating modes to allow custom tailoring of the power profile to the application requirements.

The base unit typically consumes 180 μA/MHz when executing code (note how vendors characterize this parameter to facilitate speed/power tradeoff analysis). In deep-sleep mode, current drain is 900 nA, and in shutoff mode, it is just 20 nA. The wakeup transition is also fast and thus power stingy, registering at just 2 μs.

Other representative units are in the PIC family from Microchip Technology Inc. The PIC24F32KA304 microcontroller, for example, needs just 20 nA in deep sleep, 25 nA in sleep mode with RAM retention (note that even 5 nA is considered significant), and 500 nA in sleep mode with the real-time-clock (RTC) and calendar functions enabled. Further, it wakes up in 1 μs and uses just 500 μA/MHz.

What about testing?

Budgeting and subsequent planning are essential, of course, but normally must be verified by testing and confirmation. For energy-harvesting designs, however, testing is so challenging that extra effort in the up-front stages is even more important. Testing is difficult for several reasons:

  • The energy source is minute and erratic.
  • You are trying to measure tiny current values. At these levels, conventional techniques such as using a sense resistor (current shunt) and oscilloscope, will significantly affect both reading accuracy and system performance.
  • Most ammeters and DVMs use a long integration time to measure microamperes and lower currents. Since energy-harvesting designs often are in short-cycle modes on both the harvest and load sides, this integration makes it very challenging to obtain valid readings for lower-power sleep/quiescent/transition modes and especially the higher-power active-state mode.
Therefore, it is important to work out a test plan and budget for the design if your bench does not have the specialty instrumentation needed, nor the techniques used for extreme-low current, burst-mode current drain and power use.

Summary

Energy harvesting – perhaps better described as "scavenging"– is now a practical way to provide long-term power for data logging and other low-rate, limited-range applications. However, while it may appear to offer something for "almost free," a successful harvesting design requires careful budgeting of collected energy, power use, duty cycle, and operational modes of the overall circuit and design. This article examined some of the numbers and described how to balance the budget for a successful implementation, as well as presented some of the trade-offs and choices the designer faces.

聲明:各作者及/或論壇參與者於本網站所發表之意見、理念和觀點,概不反映 DigiKey 的意見、理念和觀點,亦非 DigiKey 的正式原則。

關於作者

Image of Bill Schweber

Bill Schweber

Bill Schweber 是電子產品工程師,至今已撰寫三本有關電子通訊系統的教科書,以及數百篇技術文章、評論專欄,及產品特色介紹。他曾擔任 EE Times 的多個特定主題網站的技術網站管理人,以及 EDN 的執行編輯和類比技術編輯。

在類比和混合式訊號 IC 領導廠商 Analog Devices, Inc. 任職期間,Bill 從事行銷溝通 (即公關) 職務,因此他在技術及公關職能兩個方面皆有實務經驗,能與媒體雙向交流公司產品、業務事例及傳遞訊息。

Bill 在加入 Analog 從事行銷溝通職務前,原在業界舉足輕重的技術期刊擔任副主編,也曾任職於該公司的產品行銷和應用工程團隊。在此之前,Bill 於 Instron Corp. 從事材料測試用機器控制的類比電路和電源電路設計以及系統整合。

他擁有麻薩諸塞大學電機工程碩士學位和哥倫比亞大學電機工程學士學位,為註冊專業工程師,並持有進階級業餘無線電執照。Bill 也曾就各類工程主題進行線上課程的規劃、撰寫及講授,包括 MOSFET 概論、ADC 的選擇以及驅動 LED。

關於出版者

Electronic Products

Electronic Products 雜誌和 ElectronicProducts.com 網站能為工程師與工程管理人員在設計電子設備與系統時提供資源。