Olimex LTD 的 MOD-WIFI-ESP8266 Reference 規格書

OUMSC CHANGING THE MODES OF MOD-WIFI-ESP8266 ®, lead-free
CHANGING THE MODES OF
MOD-WIFI-ESP8266
REFERENCE
Revision A, January 2015
Designed by OLIMEX Ltd, 2014
All boards produced by Olimex LTD are ROHS compliant
OLIMEX© 2014 MOD-WIFI-ESP8266 reference
DISCLAIMER
© 2015 Olimex Ltd. Olimex®, logo and combinations thereof, are registered trademarks of Olimex Ltd. Other product
names may be trademarks of others and the rights belong to their respective owners.
The information in this document is provided in connection with Olimex products. No license, express or implied
or otherwise, to any intellectual property right is granted by this document or in connection with the sale of
Olimex products.
This work is licensed under the Creative Commons Attribution-ShareAlike 3.0 Unported License. To view a copy of
this license, visit http://www.creativecommons.org/licenses/by-sa/3.0/.
This hardware design by Olimex LTD is licensed under a Creative Commons Attribution-ShareAlike 3.0 Unported
License.
The software is released under GPL.
The product described in this document is subject to continuous development and improvements. All particulars of the
product and its use contained in this document are given by OLIMEX in good faith. However all warranties implied or
expressed including but not limited to implied warranties of merchantability or fitness for purpose are excluded. This
document is intended only to assist the reader in the use of the product. OLIMEX Ltd. shall not be liable for any loss or
damage arising from the use of any information in this document or any error or omission in such information or any
incorrect use of the product.
This evaluation board/kit is intended for use for engineering development, demonstration, or evaluation purposes only
and is not considered by OLIMEX to be a finished end-product fit for general consumer use. Persons handling the
product must have electronics training and observe good engineering practice standards. As such, the goods being
provided are not intended to be complete in terms of required design-, marketing-, and/or manufacturing-related
protective considerations, including product safety and environmental measures typically found in end products that
incorporate such semiconductor components or circuit boards.
Olimex currently deals with a variety of customers for products, and therefore our arrangement with the user is not
exclusive. Olimex assumes no liability for applications assistance, customer product design, software performance, or
infringement of patents or services described herein.
THERE IS NO WARRANTY FOR THE DESIGN MATERIALS AND THE COMPONENTS
USED TO CREATE MOD-WIFI-ESP8266. THEY ARE CONSIDERED SUITABLE ONLY
FOR MOD-WIFI-ESP8266.
Page 2 of 4
Mun- iFi-ESFEZSS, boird revision A narnuare smr jumpevs: uuu.uun:x.cor, n, ’ mno (CT 2811' N'ME» , GPIOZ ‘ < gpioo="" yhi:="" 13h]:="" provide:="" inform-{inn="" abauf="" the="" different="" mode:="" and="" jumpgr="" posiiiuna="" mode="" jumper="">
OLIMEX© 2014 MOD-WIFI-ESP8266 reference
ESP8266 has three modes of operation: SDIO mode, UART mode and FLASH
mode. By default the board is configured for FLASH mode operation. The
jumpers for the default FLASH mode were set during production as follows:
MTD0 is set to position 0; GPIO0 is set to position 1; GPIO2 is set to
position 1.
To access the other modes you would need to manipulate the on-board SMT
jumpers called MTD0, GPIO0, and GPIO2. They are located at the bottom of
the board near the UEXT connector. Each of the jumpers can be set to
either position 0 or position 1. The jumpers are highlighted on the
picture below:
The positions for the all the modes are printed on the board itself. The
table looks like this:
MODE
JUMPER MTDO GPIO0 GPIO2
SDIO 1 x x
UART 0 0 1
FLASH (DEFAULT) 0 1 1
For example:
Initially, you can't update the firmware of MOD-WIFI-ESP8266 since by the
board starts in the default FLASH mode. In order to update the firmware
of the board you would need to change the starting mode to UART. This is
done by changing the position of the jumper named GPIO0 to 0. After the
update is done – change the position of GPIO0 back to 1 again.
In order to change the position of an SMT jumper like that you would need
basic soldering skills. There are two things that you would need to do:
Page 3 of 4
OLIMEX© 2014 MOD-WIFI-ESP8266 reference
1. Remove the original connection between the pads. If it was made using
soldering – unsolder it and remove the soldering residue. If it was a
hardware PCB connection – make sure to cut between the pads with a sharp
tool (like a safety cutter).
2. Connect the pads of the desired position by soldering. Do not use a
large amount of soldering residue. Do not keep the soldering iron pressed
to the board longer than 10 seconds. Make sure that there is no left-over
soldering residue which might lead to accidental short-circuits.
If you want, you can add wires and a PTH jumper or a slide switch to the
pads of the jumpers. This would allow easier change of the jumpers in
future.
More details about the three different modes might be found in the
ESP8266 datasheet.
Page 4 of 4